Adding a Node Manager
Adding a node manager to the Node Manager-Administration panel provides a comprehensive list of installed product nodes on your machine. This panel offers centralized control for managing installed Proficy product(s).
- Log into Configuration Hub with Proficy Authentication credentials.
The NAVIGATION panel appears.
- In the NAVIGATION panel, select
Administration.
The Node Manager and License Server panels appears.
- Select Node Manager.
The Node Manager-Administration panel appears displaying the Configuration Hub and Proficy Authentication product details.
- Select
to add the Node Manager.
The Add Node Manager window appears. Enter the following details:- HOST NAME: The name of the node server where the product is installed. In the <Fully Qualified Domain Name> format.
- DISPLAY NAME: The display name is automatically populated, reflecting the host name field. You can choose to edit the display name as needed.
- PORT NUMBER: The node manager port number where the product is installed.
- If the root certificate of the Node Manager is not trusted:
- Click
Not trusted.
The Certificate Details page appears.
- Click Trust.
The root certificate is
Trusted.
- Click
- Select Add.The Node Manager added successfully message appears.Note: You can select
of the Node Manager row to view the product(s) installed on the node machine. Refer to Product Details and Actions under Node Manager for more information.
Additionally, within the DETAILS panel, you can manage product details, license activation, certificate details, and other necessary information. Refer to Node Manager Details and Actions for more information.