Items: Guidelines
About this task
Item Identifiers
- Processing of Item Identifier points works in the following manner:
Procedure
- The first character of the point value is checked when the point value is received.
-
If the first character:
Is not $ The point is expected to contain the configured identifier and that Item is searched for and moved. Is $ The rest of the value is checked against the reserved words. If the rest of the value is:
Found to be a reserved word The corresponding action is taken Not found to be a reserved word The rest of the value is taken as an Item Type ID and processing continues as if an Item Type detector was activated. -
If an Item identifier or Item type identifier is set and the Item cannot be found, an Item with that ID, reference ID or type (as appropriate) is created.
- Currently, the only reserved word is TMOUT, and the action taken is to ignore the point.
- An automatic item identifier is equivalent to a user transaction or an application interface message, in that it provides PRT with positive unique identification of the item.
If more than one entry transition indicator feeds a tracking region, items are stored in the region in the order in which the entry transition indicators are received by PRT.