Item Attributes: Defined
In the PRT database, an item is simply a record and the attributes are fields in the record that you configure, such as color or model number.
Attributes:
- Are configured by the user.
- Can change during the production process.
- Provide information that enables positive identification of an item and its location.
- Can be dynamically created from one item when it is associated with another.
Example
The following diagram shows how an item can dynamically become an attribute of another item during production.
In a sample automobile factory six and eight-cylinder engines are being tracked, along with two and four-door car frames. These are all serialized items that are positively identified through the production process.
When the engine is inserted into a car frame, the engine dynamically becomes an attribute of that car frame in the tracking system.
1 | The 6-cylinder engine is a serialized item. |
2 | The 2-door car frame is a serialized item. |
3 | The 6-cylinder engine is a: |
|
- Region(s)
- Item class
- Various item attributes criteria
An item is included in a count if its attribute matches a configured set of criteria. In order for an item to be included in the count, the attribute value must be compared against a user-defined value.