Production Tracking Configuration
It is strongly recommended that you design a tracking model that meets your company's requirements before you configure the PRT database using the Tracker Configuration User Interface (TrackerCfg_UI).
You can easily configure your database using the Tracking Model Wizard that walks you through each step of the configuration process. Properties for your regions, groups, items and the rest are all set using familiar dialog boxes in one contained structure.
You can also open any of the configuration dialog boxes at any time through the PRT tree .
Steps that describe PRT configuration using the Tracking Model Wizard include:
Step 1 | Enable the Tracker Configuration User Interface for PRT. |
Step 2 | Start the Tracking Model Wizard. |
Step 3 | Configure regions. |
Step 4 | Configure routes. |
Step 5 |
Configure item types. These items may:
|
Step 6 | Configure PRT Services. |
Step 7 | Configure system definitions. |
Step 8 | Finish basic Tracking Model configuration. |
Step 9 | Do additional Tracking configuration. |
Step 10 | Use Tracker configuration tools. |