Life Cycle Cost Analysis

Deploy LCC for the First Time

Before You Begin

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.

These tasks may be completed by multiple people in your organization. GE Vernova recommends, however, that the tasks be completed in the order in which they are listed.

Results

Step Task Notes
1Assign Security Users to one or more of the Life Cycle Cost Analysis (LCC) Security Groups and Roles.This step is required.

Upgrade or Update LCC to V4.6.11.0.0

Before You Begin

The following tables outline the steps that you must complete to upgrade this module to V4.6.11.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

Procedure

  • Upgrade from any version V4.6.0.0.0 through V4.6.10.0.0

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.5.0.0.0 through V4.5.0.0.21

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.4.0.0.0 through V4.4.0.0.16

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.3.0.0.0 through V4.3.1.0.11

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.2.0.0 through V4.2.0.9.5

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

LCC Security Groups

The following table lists the baseline Security Groups available for users within this module, as well as the baseline Roles to which those Security Groups are assigned.

Important: Assigning a Security User to a Role grants that user the privileges associated with all of the Security Groups that are assigned to that Role. To avoid granting a Security User unintended privileges, before assigning a Security User to a Role, be sure to review all of the privileges associated with the Security Groups assigned to that Role. Also, be aware that additional Roles, as well as Security Groups assigned to existing Roles, can be added via Security Manager.
Security GroupRoles
MI LCC Administrator

MI APM Viewer

MI Strategy User

MI Strategy Power

MI Strategy Admin

MI LCC User

MI Strategy User

MI Strategy Power

MI LCC ViewerMI APM Viewer

The baseline family-level privileges that exist for these Security Groups are summarized in the following table.

FamilyLCC AdministratorLCC UserLCC Viewer
Entity Families
LCC AnalysisView, Update, Insert, Delete View, Update, Insert, Delete View
LCC CostView, Update, Insert, DeleteView, Update, Insert, DeleteView
LCC Cost ValueView, Update, Insert, Delete View, Update, Insert, Delete View
LCC ElementView, Update, Insert, Delete View, Update, Insert, Delete View
LCC Operating ProfileView, Update, Insert, Delete View, Update, Insert, Delete View
LCC PeriodView, Update, Insert, Delete View, Update, Insert, Delete View
LCC ResourceView, Update, Insert, Delete View, Update, Insert, Delete View
LCC ScenarioView, Update, Insert, Delete View, Update, Insert, Delete View
Relationship Families
Has Associated LCC ElementView, Update, Insert, Delete View, Update, Insert, Delete View
Has LCC MemberView, Update, Insert, DeleteView, Update, Insert, Delete View
Has LCC CostView, Update, Insert, Delete View, Update, Insert, Delete View
Has LCC Cost ValueView, Update, Insert, Delete View, Update, Insert, Delete View
Has LCC ElementView, Update, Insert, Delete View, Update, Insert, Delete View
Has LCC Operating ProfileView, Update, Insert, Delete View, Update, Insert, Delete View
Has LCC Period View, Update, Insert, Delete View, Update, Insert, Delete View
Has LCC ScenarioView, Update, Insert, Delete View, Update, Insert, Delete View