Asset Strategy Optimization

Deploy ASO for the First Time

Before You Begin

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.

These tasks may be completed by multiple people in your organization. GE Vernova recommends, however, that the tasks be completed in the order in which they are listed.

Results

Step

Task

Notes

1Assign Security Users to one or more of the ASO Security Groups and Roles.This step is required.

Upgrade or Update ASO to V4.6.11.0.0

Before You Begin

The following tables outline the steps that you must complete to upgrade this module to V4.6.11.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

Procedure

  • Upgrade from any version V4.6.0.0.0 through V4.6.10.0.0

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.5.0.0.0 through V4.5.0.0.21

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.4.0.0.0 through V4.4.0.0.16

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.3.0.0.0 through V4.3.1.0.11

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.2.0.0 through V4.2.0.9.5

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.1.0.0 through V4.1.7.4.0

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V4.0.0.0 through V4.0.1.0

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V3.6.1.0.0 through V3.6.1.7.5

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V3.6.0.0.0 through V3.6.0.12.9

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V3.5.1 through V3.5.1.12.3

    This module will be updated to V4.6.11.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.

  • Upgrade from any version V3.5.0 SP1 LP through V3.5.0.1.10.1
    StepTaskNotes
    1Move to the Asset Strategy family any custom rules that are defined for the following families and configured to be executed during the Asset Strategy activation process: Action, Risk, Risk Assessment, Risk Rank, Action Revision, Risk Revision, Risk Assessment Revision, and Strategy Revision.This step is required.
    2Move to the Asset Strategy Template family any custom rules that are defined for the following families and configured to be executed when a new Asset Strategy Template is saved after being created from an existing Asset Strategy Template or Asset Strategy: Action, Risk, Risk Assessment, Risk Rank, and Has Risk Category.This step is required.
    3Move to the Asset Strategy or Asset Strategy Template family (as appropriate) any custom rules that are defined for any other family and are configured to be executed when an Asset Strategy or Asset Strategy Template is deleted.This step is required.
  • Upgrade from any version V3.5.0 through V3.5.0.0.7.1
    StepTaskNotes
    1Move to the Asset Strategy family any custom rules that are defined for the following families and configured to be executed during the Asset Strategy activation process: Action, Risk, Risk Assessment, Risk Rank, Action Revision, Risk Revision, Risk Assessment Revision, and Strategy Revision.This step is required.
    2Move to the Asset Strategy Template family any custom rules that are defined for the following families and configured to be executed when a new Asset Strategy Template is saved after being created from an existing Asset Strategy Template or Asset Strategy: Action, Risk, Risk Assessment, Risk Rank, and Has Risk Category.This step is required.
    3Move to the Asset Strategy or Asset Strategy Template family (as appropriate) any custom rules that are defined for any other family and are configured to be executed when an Asset Strategy or Asset Strategy Template is deleted.This step is required.
  • Upgrade from any version V3.4.5 through V3.4.5.0.1.4
    StepTaskNotes
    1Move to the Asset Strategy family any custom rules that are defined for the following families and configured to be executed during the Asset Strategy activation process: Action, Risk, Risk Assessment, Risk Rank, Action Revision, Risk Revision, Risk Assessment Revision, and Strategy Revision.This step is required.
    2Move to the Asset Strategy Template family any custom rules that are defined for the following families and configured to be executed when a new Asset Strategy Template is saved after being created from an existing Asset Strategy Template or Asset Strategy: Action, Risk, Risk Assessment, Risk Rank, and Has Risk Category.This step is required.
    3Move to the Asset Strategy or Asset Strategy Template family (as appropriate) any custom rules that are defined for any other family and are configured to be executed when an Asset Strategy or Asset Strategy Template is deleted.This step is required.

ASO Security Groups

The APM Asset Strategy Optimization module leverages the baseline APM Asset Strategy Management Security Groups. To use ASO, a user must be a member of one of the following Security Groups:

  • MI ASM Administrator
  • MI ASM Analyst
  • MI ASM Reviewer
  • MI ASM Viewer