Deploy GE Digital APM for the First Time
Deploy GE Digital APM for the First Time
The following table outlines the steps that you must complete to deploy and configure GE Digital APM for the first time. After you have completed these steps, you will need to perform additional steps to configure the modules that you have purchased.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed. All steps are required unless otherwise noted.
Step |
Task | Notes |
---|---|---|
1 | Ensure that your system meets the hardware and software requirements for the basic GE Digital APM system architecture. | This step is required. |
2 | Review how the operating systems are configured in the GE Digital APM testing environment. | This step is required. |
3 | Configure GE Digital APM Server roles and features. | This step is required. It is recommended that you configure your system to match the configuration used in the GE Digital APM testing environment. |
4 | Install the GE Digital APM Server and add-ons software on each computer that will serve as a GE Digital APM Server. | This step is required. |
5 | Install Redis on the GE Digital Redis server (Linux server). | This step is required. Note: The last supported Redis version for Windows contains Common Vulnerabilities and Exposures (CVE). Therefore, we recommend that you install Redis on a Linux server. However, if you want to install Redis on a Windows server, refer to the Install Redis on the GE Digital APM and Redis server (Windows server) topic. |
6 | Install Elasticsearch on a dedicated server. | This step is required. You must install Elasticsearch on a server in your environment. |
7 | Install ActiveMQ on a dedicated server. | This step is required. You must install ActiveMQ on a server in your environment. |
8 |
Deploy the GE Digital APM Database Server, which includes creating and configuring your GE Digital APM database. | This step is required. |
9 | This step is required. | |
10 | This step is required. | |
11 | This step is required. | |
12 | Deploy translations. | This step is required only if you want to use non-English translations in GE Digital APM. |
13 | Configure one of the virtual machine to execute all the scheduled jobs. | This step is required only if you have deployed the GE Digital APM in a clustered environment and you want to dedicate a virtual machine to run all the scheduled jobs. |
14 | Install the GE Digital APM mobile application on your mobile device based on one of the following operating systems: | This step is required only if you want to install the GE Digital APM mobile application on mobile devices. |
15 | Enable single sign-on for on-site or off-site authentication. | This step is required only if you are enabling single sign-on. |