Procedure
- If you have not already done so, activate the licenses for the translations you have purchased.
- On the GE Digital APM server, run the file Meridium.Version.EnableTranslations.exe, which is located on that machine in the folder C:\Program Files\Meridium\Upgrade\TranslationUnzip.
Note: To run this file, open a command prompt window, and then enter and execute the following:
C:\Program Files\Meridium\Upgrade\TranslationUnzip\ Meridium.Version.EnableTranslations.exe -l:<path to license>
-p:<PIN>
-e:<True or False>
...where <Path to license> is a valid path to the license file and <PIN> is the pin for the license file. The parameter -e is optional. <True or False> indicates whether the help files should be extracted. Specify True if you want to extract the help files and False if you do not want to extract the help files. If you do not use this parameter, the help files are not extracted.
- On the GE Digital APM server, reset IIS.
- You can now manage translations.