Create a segment requirement

You can create expressions or bind properties for many of these properties, depending on your workflow requirements.

Procedure

  1. In the navigator, click Workflow > Workflows.
  2. In the resource list, select the workflow that you want to work with. If no workflow exists, create a new workflow.
  3. In the Displays panel, click Workflow Management > Workflow Editor.
  4. Click the Workflow Editor tab.
  5. Insert an activity:
    • At the workflow level:
      • From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
        Note:
        Activities can exist only between the presubprocess and postsubprocess.
    • At the subprocess level:
      • Double-click the local subprocess you want to add the activity to.
      • From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
  6. On the activity configuration panel, click Configure Method.
    The Configure Method dialog box appears, displaying a list of the available call method service providers.
  7. Double-click IProductionRuntime to display the list of available call methods.
  8. Click CreateSegmentRequirement, and then click Finish.
    The input parameters appear in the activity configuration panel.
  9. In the Name field, enter a name for the segment requirement, or bind a property or parameter to the method.
  10. In the Order field, enter an execution order for the segment requirement, or bind a property or parameter to the method.
  11. Optional: In the Parent Requirement ID field, enter the ID of the parent segment requirement that the segment requirement is associated with.
  12. In the Work Definition Segment field, click the ellipsis button, and then select a work definition segment.
    The segment requirement uses this definition to define properties and hierarchy.
  13. In the Work Request field, click the ellipsis button, and then select a work request.
    The segment requirement will be associated with this work request.
  14. Click Save.
  15. Run the workflow, or, on the Test/Debug tab, test the workflow to ensure that your input parameters are configured correctly.