Configure Parameters for a Call Method
You can configure parameters for a selected call method.
About this task
Use this procedure to configure parameters for any call method.
Procedure
- In the navigator, select , and then create a new Workflow or select a Workflow from the list.
- From the Displays panel, select .The Workflow Editor page appears.
- Select the Workflow Editor tab.
- From the process map, choose from the following:
- Select Local/Global Subprocess from the Standard Activities menu, and then drag it onto the Workflow diagram to create a new subprocess.
- Double-click an existing Subprocess to display it in the editor.
- From the subprocess map, choose from the following:
- Select Call Method from the Standard Activities menu, and then drag it onto the Subprocess diagram to create a new call method.
- Select an existing Call Method to display it in the editor.
The parameters for the call method appear in the configuration panel. - Click Configure Method in the configuration panel.The Configure Method dialog box appears.
- From the Navigate tab, select a call method from the list.Note:You can select Next to display the parameters configuration panel for the selected call method.
- Click Finish.The selected call methodappears below Method in the configuration panel.
- Enter or edit values for each parameter in the selected call method, and then click Save.
- Click Run (
) to run the Workflow and the configured call method.