Configure a display in a host application

Before you begin

Note:
At a single workstation, only one Task Indicator object and one ActiveX Task List object can be connected at a time per HMI application instance.

Procedure

  1. In your host application, add an OLE object. For more information, see the host application's online help.
  2. To create a control, select:
    • Proficy Task List Control, or
    • Proficy Task List Indicator Control.
  3. To configure the control's properties, right-click the control, and then:
    Select...To enter or modify...
    EquipmentNamethe name for a linked piece of equipment to be used in the Task List.
    Note:
    This name must match the S95 ID for the equipment found in the Universal Browser. For more information, see Add a resource to the equipment model.
    ProficySOALoginUsera login user name.
    Tip:
    Property configuration is not required for Manual Login.
    ProficySOALoginPassworda login password.
  4. Configure your host application to handle selected events.