Change the active layer
By default, the top-level active layer is a grid control.
Procedure
- In the navigator, click .
- In the Folders list, select the resource type you want to work with.
- Click .
- If required, add a control that can be set as the active layer by clicking Toolbox and expanding the group you want to work with.
- Click and drag the control to the desired position in the Designer.Note:To apply the properties of a control to another control, click and drag the control to another control in the document tree. The Applying <control (control name)> to Target dialog box appears where you can select the option you want to use to apply to the control.
- Right-click the control in either the Designer or the document tree, and then select Edit Layer.
- Or -
Double-click the control in the document tree.The control displays in the designer with an orange border, indicating that it is the active layer. - Add controls to the active layer, as required.When you make another control the active layer, you cannot select the controls that were added in other active layers because they are now part of an inactive layer. In order to change these controls, you must make that layer active again.
- Save the form or user display.
Click Save on the... To save... toolbar locally for WPF forms; to the server for Silverlight forms title bar to the server for WPF forms