Add an OPC UA Server
You can connect to an OPC UA server that is installed on your application server computer.
About this task
Before you can add an OPC UA Server, you will need to generate a Workflow certificate and register it with the GDS server. For more information, see Register Workflow Certificates with Global Discovery Server (GDS).
Procedure
- In the navigator, click .
- Click Add OPC UA Server.
- In the Name field, enter a name for the OPC UA server to which you want to connect.
- Optional: In the Description field, enter a description of the OPC UA server.
- Click OK.