Subscription Data Form
The subscription data form allows you to retrieve a directory resource, when defined conditions are met, to advance a workflow task.
Note:
These parameters are configured when the form is selected for a Form activity.
Inputs
The following table describes parameters for this form:
Important:
A value must be entered in the Data Item and Prompt fields.
Parameters | Data Type | Description |
---|---|---|
Auto Submit | Boolean | If True, there is no Submit button on the form when it is running. Therefore, when the input values match, the form submits automatically. If False, a Submit button appears on the form; it must be clicked to submit the form. |
Data Item | N/A | Select a resource to use as a value to check against other input parameters. |
Default Value | String | Initial value of the text field. This field can be used to introduce or clarify mask and limit information. |
Format Mask | String | Enter a mask for the subscription data value. Tip: For more information on applying masks, see the Mask Properties in the MSDN Library. |
High Limit | Double | If applicable, enter the exclusive upper limit for a numeric value. Use this field if the data being retrieved is numerical and must fall within a range to advance the form. Note: The value entered in the form must be up to the high limit value, not including the high limit value. For example, if the high limit is 100, the value cannot be higher than 99. |
Limits Visible | Boolean | If True, the high and low limits display in the form when it is running. |
Low Limit | Double | If applicable, enter the exclusive lower limit for a numeric value. Use this field if the data being retrieved is numerical and must fall within a range to advance the form. Note: The value entered in the form must be above the low limit value, not including the low limit value. For example, if the low limit is 1, the value must be higher than 1. |
Prompt | String | Enter text to provide information to an operator to perform an action. |
Outputs
The following table displays parameters for this form:
Parameters | Data Type | Description |
---|---|---|
Value as double | Double | Displays the value text. |
Value as int | Int32 | Displays the value text. |
Value as String | String | Displays the text for the value when the form is submitted. |