Server State Icons for Task Indicator
Indicator icons provide visual information about the status of the server connection, as well as the status of tasks. If configured to do so, a status message can also be displayed to provide more information to the user.
The following table describes the icons associated with the Task Indicator:
Icon | Status | The indicator is... |
---|---|---|
![]() | not connected | static when it is initially loaded or when a connection is lost. |
![]() | connecting | green and animated when it is in the process of connecting to the server. |
![]() | connected | enabled when a connection succeeds. |
![]() | task waiting | flashing when new tasks to be performed are available. |
![]() | task expired | flashing when an available task expires. |
![]() | lost connection | yellow and animated when a previously connected server loses connection. |