QueryWorkResponses (IProductionReport)
Performs a query against the runtime database for work responses based on the selected input parameters. All work responses that match the specified query criteria are returned.
In the Configure Method dialog box, click Next to select query criteria to include as input parameters on the activity configuration panel.
Inputs | Data Type | Description |
---|---|---|
Detail Level | WorkResponseDetailLevel |
Specifies the detail level of the output. Select one of the following:
|
End Time (Max) | DateTime |
Specifies the latest end date and time to include in your query. Only responses that occurred on or before this date/time are returned. In the Configure Method dialog box, click Next to specify the criteria type to use in your query. Note:
If you select Range, then the End Time (Max) and End Time (Min) parameters are
available and all responses matching the parameter inputs are returned. If you select
Not Set, then the query returns only those responses that do not have an end date/time
defined. In the Inputs section of the activity configuration panel, click the drop-down arrow to set the date and time. |
End Time (Min) | DateTime |
Specifies the earliest end date and time to include in your query. Only responses that occurred on or after this date/time are returned. In the Configure Method dialog box, click Next to specify the criteria type to use in your query. Note:
If you select Range, then the End Time (Max) and End Time (Min) parameters are
available and all responses matching the parameter inputs are returned. If you select
Not Set, then the query returns only those responses that do not have an end date/time
defined. In the Inputs section of the activity configuration panel, click the drop-down arrow to set the date and time. |
Location | DirectoryResource |
Specifies the equipment location to include in your query. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |
Origin Work Request | DirectoryResource | Specifies the originating work request to include in your query. Note: This
parameter applies only if any of the work responses you are querying have been moved
from one work request to another. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |
Response State | String |
Specifies the work response state to include in your query.
|
Segment Dtail Level | SegmentResponseDetailLevel |
Specifies the detail level of the output. Valid values are:
|
Start Time (Max) | DateTime |
Specifies the earliest start date and time to include in your query. Only responses that occurred on or after this date/time are returned. In the Configure Method dialog box, click Next to specify the criteria type to use in your query. Note:
If you select Range, then the Start Time (Max) and Start Time (Min) parameters are
available and all responses matching the parameter inputs are returned. If you select
Not Set, then the query returns only those responses that do not have a start date/time
defined. In the Inputs section of the activity configuration panel, click the drop-down arrow to set the date and time. |
Start Time (Min) | DateTime |
Specifies the earliest start date and time to include in your query. Only responses that occurred on or after this date/time are returned. In the Configure Method dialog box, click Next to specify the criteria type to use in your query. Note:
If you select Range, then the Start Time (Max) and Start Time (Min) parameters are
available and all responses matching the parameter inputs are returned. If you select
Not Set, then the query returns only those responses that do not have a start date/time
defined. In the Inputs section of the activity configuration panel, click the drop-down arrow to set the date and time. |
Work Request | DirectoryResource |
Specifies the work request to include in your query. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |
Outputs | Description | |
---|---|---|
WorkResponseCollection | Returns all of the work responses that match the query parameters. Use a For Each Activity to loop though all resources, an Index Activity with an integer value, or the name of the work response. |