Import/Export Display

The Import/Export display allows you create files containing configurations for a given type or category of Workflow resource for transfer between servers or operational environments.

The following describes the available options.

AttributeValueDescription
Content FolderUser-definedClick the ellipsis button to select a folder to export a resource configuration file to.
Content FilesUser-definedDisplays a list of resource configuration files in the selected location.
Note:
This list may not reflect all resource configuration files currently in the location. For more information, see Refresh the list of resource configuration files.
Add FileUser-definedClick to create a file to add resource configurations to.
Delete FileUser-definedClick to delete the selected resource configuration file.
RefreshUser-definedClick to update the list of resource configuration files to see all files currently in the selected location. For more information, see Refresh the list of resource configuration files.
NameUser-defined alphanumeric string (A-Z, a-z, 0-9) up to 50 charactersSpecifies a name for the resource configuration file.
DescriptionUser-defined alphanumeric string (A-Z, a-z, 0-9) up to 255 charactersSpecifies information about the resource configuration file that a user may find helpful.
Content TypeSystem-definedSelect the type of resources that you want to export configurations for. For more information, see Content-Specific Transfer Considerations.
Content DetailsUser-definedDisplays the name and description of the resources that you added configurations for in the selected file.
Add ContentN/AClick to open the Universal Browser to select the resources that you want to export configurations for.
Delete ContentN/AClick to exclude the configurations for the selected resources from the export process.
Export ContentN/AClick to send the configurations for the selected resources to the specified file in the selected folder.
Import ContentN/AClick to transfer the resource configurations in the selected file to the current system. Resource configurations that do not pre-exist on the destination system are added there; existing configurations are updated. (For more information, see Configuration Updates in General Transfer Considerations.)
Note:
Beginning with Workflow 2.2, you can import content that has been exported from previous versions of the software. For workflows, you can import content exported from version 1.5 Service Pack 2 or later; other types of content must have been exported from version 2.0 or later.