AddOPCGroup (IOpcClient)

Adds an OPC group to the specified OPC server.

Inputs Data Type Description
OPC Server DirectoryResource Specifies the OPC server under which the group is created.
Group Name String Specifies the name of the OPC group.
Group Description String Specifies the description of the OPC group.
Update Rate (ms) int32 Specifies the rate in milliseconds that the server is requested to update items in the group.
Enabled Boolean Specifies whether the group is enabled. True if so; otherwise, False.
Note:
The default is True.
Device Read Boolean Specifies whether to read directly from the device or read from the OPC server's cache. True if so; otherwise, False.
Note:
The default is True. If false, reading is performed against the OPC server's cache.
Deadband (%) Single Specifies the minimum percentage of the value range of an item that a value in the group must change to trigger a data changed event.
Outputs Description
Response Returns a response indicating creation of the OPC group.