Sounds
About this task
Webspace supports sound capability for any application that uses PlaySound, sndPlaySound, or waveOut. It is not required that sound cards and/or speakers be installed on Webspace Servers. The client machine, however, does require a sound card, speakers, and the Windows Media or Desktop Experience Feature to be enabled. Audio support is disabled by default on the Webspace sessions.
Important:
Be aware that client sound capability requires the loading of
Webspace libraries into session processes. This can affect the startup
of a process, make some processes incompatible with Webspace,
or have fatal consequences during suspend/resume operations. Use caution
when enabling this setting.
Procedure
- In the Webspace Administration, select the desired server from the list of All Servers.
- On the Tools menu, click Host Options. The Host Options dialog box appears.
- Click the Client Access tab.
- Click the Sound check box.
- Click OK.