Clipboard Access

About this task

You can cut and copy information from a Webspace session and paste it into applications running on a Webspace Server, and vice versa. Clipboard support is disabled by default.

Procedure

  1. In the Webspace Administration, select the desired server from the list of All Servers.
  2. On the Tools menu, click Host Options. The Host Options dialog box appears.
  3. Click the Client Access tab.  
  4. Click the Clipboard check box.
  5. Click OK.

    Any clipboard data from the browser session is available only within the WorkSpace application. In order to copy the contents to other applications on the local disk of the client machine you must create a shell script within an object inside your WorkSpace picture that launches Notepad.exe, on the Webspace Server. After you do this, you can use this object to launch Notepad in run mode from the web session. Paste the contents into Notepad, and save this file to the local disk of web session computer.