SEQ |
The sequence number of the operation. |
NAME |
The name of the operation. |
DESCRIPTION |
The description of the operation. |
BEHAVIOR |
The behavior of the operation. The following options are available:
- Clocking: If this option is selected, the operation requires manual clocking on and clocking off.
- Non Clocking: If this option is selected, the operation does not require a manual clocking on.
|
LABOR TYPES |
The labor type of the operation. |
DEFAULT LABOR |
The default labor type. |
EQUIPMENT |
The equipment that is used to perform the operation. There can be multiple equipment for the same operation. |