PROPERTY NAME | Denotes the name for the property. You must enter a value that is unique to a group. |
ALIAS NAME | Enter an alias for the property. |
DATA TYPES | Select a data type for the property. Note: A data type defines the format in which the data is stored and displayed in the application. |
DEFAULT VALUE | Enter a default value for the property based on the data type. |
REQUIRED VALUE | Select this check box only if you want the property to be a required value. |
PROPERTY GROUP | Displays the group name based on the selection in the GROUP drop-down list box. You cannot edit this field if you have already selected the group from the GROUP drop-down list box.Note:
- If you have selected a specific category from CATEGORY, you can select a group that is mapped to the selected category from this drop-down list box.
- If you have left CATEGORY and GROUP drop-down list boxes to defaults, this drop-down list box displays a list of groups defined in the Plant Applications database. You must select the group to which you want to assign the property.
|
UOM | This box contains a list of UOMs defined in the Plant Applications database. Select a unit of measurement (UOM) for the property. |