For an ERP application, you should use only the default groups available in the Property Definition application. However, you can create new groups for the Route Editor application. Create groups only in the category that includes the string Route in its name. You can add these property groups to a route or an operation in the Route Editor application. For more information, refer to Assign a Property Group.
Procedure
Select .
The Property Definition page appears, displaying a list of properties available in the Plant Applications Web Client.
From the CATEGORY drop-down list box, select a required category for which you want to associate this group.
Note: You can skip to step 3, if you want to create a group and not map it to a category.
From the GROUP drop-down list box, select Create New.
The Create Property Group page appears.
Enter a group name in the GROUP NAME text box and then select Create. The newly created group is added to the Group list and is mapped to the selected category.
Note: To create multiple property groups and map it to a specific category, perform the following:
From the CATEGORY drop-down list box, select a required category.
Now, perform step 3 and 4 by not changing the category for creating each group. The newly created groups are mapped to the selected category respectively.