Before you begin
If you do not have the permission to perform this task, a message appears, stating the same. If that happens, request your administrator to provide the permission using Security.
About this task
After you perform an operation on a lot, you can provide the quantity of the lot on which you have performed the operation.
You can provide the completed quantity only if the following conditions are satisfied:
- The product is non-serialized.
- The operation requires clocking on (as defined in Route Editor or the ERP system).
- You have specified the BOM consumption for all the mandatory BOM items for the quantity of the lot that you want to mark complete. For example, in a lot of eight items, if you have performed the operation on two items, you must specify the BOM consumption for the two items. The quantity of the consumed BOM items must be greater than or equal to the required quantity to perform the operation.
- You have provided data for all the mandatory quality variables for the lot that you want to mark complete.
- The lot is clocked on by you.
Procedure
-
Access the operation for which you want to provide completed quantity.
-
Select
.
Note: The

button appears only if the lot is clocked on by you.
The RECORD QUANTITY window appears.
-
Enter the quantity of the lot for which you have completed the operation. The
quantity that you enter must be less than or equal to the available quantity.
If threshold values are defined for the lot, you must enter the
quantity that satisfies the threshold range.
A lot configured with threshold limits allows the operator to
deviate from a planned quantity, and complete with more or less
quantity based on the actual execution of the lot. A threshold range
is configured for the product to identify the maximum and minimum
allowed quantity to record in a lot to complete it.Note: Record quantity is populated by default,
when
default.record.quantity.to.remaining.quantity
is set
to true. If false, you must manually enter the outstanding quantity
available for a serial/lot. This application service variable is set during
Plant Applications installation.
If you have installed Enterprise Plant
Applications Web Client, these parameters are available in the following
file:
<installation_path>/PlantApplicationsDocker/plantapps-web-docker/mnt/configfiles/operator-app-service/prod/<version>/operator-app-service-prod.properties
After
you change the values of parameters, run the following Docker commands
to restart the Operator app service:
sudo docker service scale
PAOperatorappservice_operatorappservice=0
sudo docker service scale
PAOperatorappservice_operatorappservice=1
If you have installed Standard Plant Applications Web Client, these
parameters are available in the following file:
C:\Program Files\GE Digital\PlantApplicationsWebClient\config-repo\operator-app-service\prod\<version>\operator-app-service-prod.properties
After
you change the values of parameters, restart the Operator app
service.
-
Select
Record.
Tip: If you also want to clock off the lot, select Rec + Clock Off.
-
Select any of these options:
Button | Description |
---|
Rec + Complete |
Appears only when the threshold values are configured for the lot.
- Records the actual quantity entered by the operator and
completes the lot, provided the actual quantity is within the
defined thresholds.
|
Rec + Clock Off |
- If threshold values are configured for the lot, records the
entered quantity and the operator is clocked off the lot.
- If threshold values are not configured, and
- the recorded quantity is less than the planned quantity,
then the quantity is recorded, and the operator is
clocked off the lot.
- the recorded quantity is equal to the planned quantity,
then the lot is completed, and the operator is clocked
off the lot.
|
Record |
- If threshold values are configured for the lot, records the
quantity entered by the operator.
- If threshold values are not configured, and
- the recorded quantity is less than the planned quantity,
then only records the quantity.
- the recorded quantity is equal to the planned quantity,
then records and completes the lot.
|
Results
If the completed quantity of the lot is equal to the
planned quantity, the operation is marked complete for the lot.