SUMMARY | Enter the summary of the non-conformance. A value is required. |
NON CONFORMANCE TYPE | This box is disabled and populated with the value Manufacturing Defect. |
DEFECT TYPE | Select the type of the defect associated with the non-conformance. A value is required. |
DEFECT REASON | Select Select Reason, specify the hierarchical set of reasons for the non-conformance, and then select Apply. Note: The reasons that appear in the Select Reasons window are pre-defined in Plant Applications Administrator, and appear based on the value in the NON CONFORMANCE TYPE box. If you want to modify the list of reasons, contact your administrator. |
FULL DESCRIPTION | Enter the full description of the non-conformance. |