STATUS | The status of the defect. |
SERIAL/LOT# | The serial/lot number of the defective part. You can select the link in this column to search for all the defects associated with the serial/lot. |
PLAN | The disposition plan created for the defect. You can select the link in this column to search for defects associated with the disposition plan. For a defect in the Submitted state, the value in this column is blank. |
OP | The operation during which the defect was created. |
MATERIAL | The material of the defective part. You can select the link in this column to search for defects associated with the material. |
MATERIAL FAMILY | The material family associated with the defective serial/lot. |
QTY | The quantity of the defective serials/lots for the non-conformance. For a serialized product, the value in this column is always 1. |
DISP | The method of disposition performed on the defective serial/lot. For a defect in the Submitted status, the value in this column is blank. |
CTP/REWORK OP | The operation until which a defective serial/lot can be processed before disposing the defect. This is applicable only if the disposition method for the defect is Continue-to-Process (CTP). During the operation specified in this column, the defect must be disposed. |
MATERIAL DESC | The description of the material of the defective serial/lot. |
DEFECT REASON <number> | The hierarchy of reasons identified for the defect. |
ACTION REASON <number> | The hierarchy of actions identified for the defect. |
ACTIONS | The actions that you can perform on the serial/lot. Contains the following buttons: : Select this button to dispose the defect. This button is enabled only for a defect in the Submitted status. : Select this button to modify the non-conformance details. This button is enabled only for a defect in the Submitted status. : Select this button, and then select Remove from Plan to remove the defect from a disposition plan.
|