Sort Notifications by | Select one of the following options to decide the order in which alarm notifications appear in the Notifications pane:- Priority: Select to access alarm notifications sorted by decreasing order of alarm priorities; that is, high priority alarms appear first, followed by medium priority alarms, and then low priority alarms.
Note: You set priority of an alarm notification in the alarm template in Plant Applications Administrator. - Time Received: Select to access alarm notifications sorted chronologically by the date (and time) when they were received; that is, any new alarm notification will appear first.
Note: By default, the alarm notifications are sorted by time received.
|
View Alarms By | Select one of the following options to view alarms only in the selected time range option, product, or process order:- Current Shift: Select to access all alarm notifications associated with activities in the ongoing shift.
Note: By default, this option is selected.
- Current and Previous Shift: Select to access all alarm notifications associated with activities in the ongoing shift and from the shift prior to the current shift.
- Current Day: Select to access all alarm notifications associated with activities on the current Production Day.
Note: If shifts are not configured, this option is selected by default. - Current and Previous Day: Select to access all alarm notifications associated with activities on the current Production Day and from the day prior to the current Production Day.
Note: The Previous Shift and Current and Previous Shift options appear only when shifts are defined for the Display in Plant Applications Administrator. |
Dismiss Float Alarm Notification in | Enter a duration in seconds after which the float alarms notifications disappear. Note: By default, the box value is set to 5 seconds. |
Until I Close Manually | Select to close the float alarm notification window manually. Note: If you select this check box, the Dismiss Float Alarm Notification in is disabled. |