This topic provides a list of common tasks that you can perform using Plant Applications Web Client.
Add or Remove Columns
When you access an application, by default, a few columns appear. You can remove some of these columns or add new ones. To do so, select

.
- To add a column, select the corresponding check box.
- To remove a column, clear the corresponding check box.
Filter Records
You can filter records based on a single search parameter or multiple search parameters.
- If you want to filter records based on a single search parameter, in the column that contains the parameter, select
. - If you want to filter records based on multiple search parameters, select
.
E-Signature Authentication Icon
When the Performer session is active, as a Performer, you can see the
icon is activated in the Activities, Work Queue, and Unit Operations application pages. If you need to leave your workstation for a brief period, you can select the
to ensure that any additional changes will require performer authentication. This helps prevent unauthorized changes.Group Records
You can group records based on the values that appear in a column. To do so, drag the column heading to the page heading. For example, in Work Order Manager, if you want to group work orders based on the material, drag the MATERIAL column heading to the page heading. A list of work orders for each material appears.
Add or Modify Autolog Variables Values in Offline Mode
In the
Activities application, if you are in the process of adding or modifying the values of the autolog variables, and the system goes offline, you can continue to add or modify the value of the variables. However, the autolog sheet is updated only when the connectivity is restored.
Note: When the system is offline, you will not have access to the rest of the Plant Applications Web Client.