Modifications and Additions to Properties in Plant Applications Web Client 8.1
Plant Applications 8.0 | Plant Applications 8.1 | Comment |
---|---|---|
ROUTE_WORKORDER_CATEGORY | ERP APP | ROUTE_WORKORDER_CATEGORY is removed in Plant Applications 8.1. The ERP application is added in Plant Applications 8.1 to consolidate ERP related groups under one category. |
ROUTE_WORKORDER_GROUP | WorkOrder Import | ROUTE_WORKORDER_GROUP is renamed WorkOrder Import. Any properties configured in the older group are moved to the new group during installation. The ERP application uses the properties from the new group while creating a work order. |
ROUTE_MATERIAL_CATEGORY | ERP APP | The category of properties is removed from Plant Applications 8.1. |
ROUTE_MATERIAL_GROUP | Material Import | ROUTE_MATERIAL_GROUP is renamed Material Import. Any properties configured in the older group are moved to the new group during installation. The ERP application uses the properties from the new group while creating material. |
- | MaterialLot Import | Added in Plant Applications 8.1. The ERP application uses the properties from this group while creating a material lot. |