Update or Validate the Database Password
About this task
This tab allows you to update the database password the Web Client uses to connect to the Plant Applications databases. You can also use this tab to validate the current database password.
You can validate or update the database credentials in the Web Client.

Procedure
-
To validate the current credentials in the Web Client, do this:
- Enter the Current Username and Current Password in the respective fields.
- Select Validate.
If the details provided are valid, a Successfully Validated message appears.
-
To update the database credentials in the Web Client, do this:
- In the Update Database Credentials in Web Client section, enter the required information in the Username, Password, and Confirm Password fields.
- Select Update.
If both the latest and current passwords are the same, a confirmation message appears.
- Select Yes to confirm.
A confirmation message appears for resetting the password.
- Select Yes to update all the .war files with the latest password.
The configuration process might take up to 15 minutes. When the password is successfully reset, the message appears: Password is successfully reset.