Search Browser
About the Search Browser
Use the Search Browser to search for assets tags, and correlated tags for the enterprise.
- name: tag instance name.
- sourceKey: tag unique identifier.
- inContext: asset context.
- ofClass: tag classification name.
- <attributeName>: tag attribute value.
You can enter multiple search criteria based on the modifiers, adding them to the Search box. You can type the characters of the criteria or copy from another location and paste the characters in the Search box.
- When you type the special characters asterisk (*), colon(:), and backslash(\) in the Search box as part of the search criteria, you must type a backslash(\) before these characters to escape them. Else, the specific special characters are displayed as different characters than expected. However, when you copy and paste tag names with the specific special characters in the Search box, the backslash(\) is added before the specific characters by default. You do not have to add the backslash(\) before the special characters manually to escape them.
- Wildcard search and usage of modifiers is not supported on the paste functionality for asset tags search.
The Search button is enabled only when any search criterion is added to the Search box. The Search button is disabled after the search is triggered until a new criterion is added or any existing criteria is modified.
If you enter more than 10 search criteria, you can scroll down the Search box to view the criteria.
Hovering over the search criteria chip displays an information tooltip prompting you to double click the chip to edit the search criteria or click to clear the criteria.
A maximum of 250 results is displayed at a time. You can select the maximum number of results to be displayed per page, 40 or 100, using the results per page drop-down list box. On the pagination toolbar, when the first page is selected is disabled and when the last page is selected
is disabled.
If all the results appear on one page, the Select All check box appears on the Search Browser. You can select all the tags from the search results to add to a chart, by selecting this check box.
If the results appear on multiple pages, the Select Visible Tags check box appears on the Search Browser. You can select all the visible tags on the page to add to a chart by selecting this check box.
The search results header displays the number of search results that are selected.
Correlated tags and units of measure are displayed in the search results for a tag when available. Hovering over a tag or a correlated tag in the search results displays an information tooltip. Tooltip information is not displayed for nodes. Tags and correlated tags can be dragged to a chart for plotting.
If you drag a tag associated with an asset that is not currently displayed in the Tag Tree Browser from the search results to a chart, that asset and its associated tags display in the Tag Tree Browser.
You cannot add additional assets for Event Data Analysis charts from the Tag Tree Browser, Tag Expressions or Search Browser panes.
Search for Asset Tags
Use the Search Browser to search for enterprise asset tags using modifiers.
About This Task
You can search for asset tags belonging to assets that are not on the Tag Tree Browser. Use the search modifiers to narrow your search.
Procedure
Search for Correlated Tags
Use the Search Browser to search for correlated tags associated with asset tags.
About This Task
You can search for correlated tags associated with asset tags. Use the search modifiers to narrow your search.
Procedure
Search Using Modifiers
Use search modifiers to narrow displayed tags by categories.
About This Task
You can enter a few characters into the Search box to display all tag names or source key information that matches those characters within the enterprise. Instead of entering a tag name into the Search box, you can string modifiers together to narrow your search to a few specific tags.
For more information on the search modifiers and their results, refer to the Search Modifiers topic.
Procedure
- In the module navigation menu, select .
- Use the Context Browser to select an asset context.
- In the View Selector, select a Public Templates or My Templates view.
- In an existing chart, select
on the Tag Tree Panel.
- Select Search Help to display the allowable modifiers below the Search box.
- Enter one or more modifiers in the Search box to display all tags related to the criteria, then select Search.
Stringing modifiers
In this example, suppose you enter the following modifiers: inContext:BFP_1, ofClass:Turbines, UoM:ohm, BR1X.
The results are tags that have BR1X anywhere in their name, that are associated with the BFP_1 asset, are part of the Turbine class, and use ohms as their unit of measure. Correlated tags for each displayed tag in the search are also found.