Analysis Templates
About Analysis Templates
Analysis templates are created by naming the template, adding cards and charts, and then saving them. You can view a saved analysis template using the View Selector.
Analysis templates allow you to create customized charts for the time series data that is stored in Predix Time Series or a central Historian / OSM. An Analysis template allows you to organize the charts in logical groups within the cards and associate them with various asset instances or classifications across the hierarchy. The Analysis templates can also be associated with an alert or case, or used to compare events across time to analyze the degradation of an asset.
The Analysis view controls the primary asset context and date range that allows you to select between saved views. Each view contains at least one card, which in turn contains at least one chart. Analysis views consist of an Alert Analysis view redirected from the Alerts module, or a Time Series Analysis or Event Data Analysis view.
You can set a default Analysis view with an asset that allows you to load the default visualization for an asset. The default Analysis template exists for both SmartSignal Analytics and non-SmartSignal Analytics.
When you select an Analysis view, the first card in the view, containing up to four charts, appears. You must select the button to access additional cards.

- Display the tag aliases for tags.
- Show template information.
- Add a card to the view.
- Export data on the view as a CSV file.
- Save or update the view as a new template.
- Delete a template.
- Connect all the remaining data points after filter is applied to all the time series charts.

- Change your personal time preferences.
- Select a chart resolution.
- Select a data source.
Selecting the button accesses the Tag Tree panel. As you add cards to your view, the Jump Menu is enabled, allowing you to jump to a card in the list.
When you save a view as a template, the Context Ribbon appears. Using the Context Ribbon, you can name the template, designate the template as public or private, and select between class and instance templates.
Change the Time Preference Settings
You can view assets based on time zone.
About This Task
When looking at chart data, you may want to view the data in the local time zone for a customer or asset.
- The Date Picker dates.
- The date and time on the x-axis.
- The chart Timeline Slider.
- The Chart Register timestamps and time zone designation.Note: The Chart Register and Timeline Slider do not appear in the Event Data Analysis view.
- UTC (universal time zone)
- Site Local
- User Preference
Procedure
Select the Chart Resolution
To refine the view for data in a selected date range, you can increase or decrease the number of data points sampled on charts for a selected date range.
About This Task
When you create a Time Series Analysis or Event Data Analysis, you can select the chart resolution for the selected asset context. Predix Essentials limits the data points for larger date ranges to manage readability and performance. Changing the resolution affects all charts in the view.
Data resolution is saved when you save the chart as a template.
Chart resolution is calculated as one data point per interval. For example, selecting 10 sec data (max 1 day) results in a calculation of 86,400 seconds in a day, divided by 10 seconds. This determines the maximum of 8,640 points permitted in the chart.
All charts use a default resolution of 1000 points per tag.
- Default Data Resolution
- 1 hr data (max 2 years)
- 30 min data (max 2 years)
- 10 min data (max 1 year)
- 5 min data (max 92 days)
- 1 min data (max 30 days)
- 10 sec data (max 14 days)
- 5 sec data (max 7 days)
- 2 sec data (max 2 days)
- 1 sec data (max 1 day)
- Raw Data
Procedure
- In the module navigation menu, select .
- Use the Context Browser to select an asset context.
- Complete one of the following actions:
- In the View Selector, select New Time Series Analysis or New Event Data Analysis, and then select a chart type in the Chart Type box.
- In the View Selector, select a Public Templates or My Templates view in the available options.
- In an Alert Detail page, select an Analysis icon in the Analysis section to view an Alert Analysis chart.
- Select a date range in the From and To boxes.
- Modify the chart and plot tags as needed.
- In the Data Resolution drop-down list, select an option.
Select a Data Source
You can select a time series data source when you create a chart.
About This Task
When looking at chart data, you may want to view the data in the source OSM system, especially when isolating trips. This capability allows you to switch the data source for a view.
When you create a Time Series Analysis or Event Data Analysis chart in the Analysis view, you can select a data source for the selected asset context.
The options available in the Data Source box in Analysis views are determined by the selected asset in the Time Series Data Sources module.
The selections available in the Data Source box populate when you select the options menu.
Procedure
Select a System of Measure
About This Task
- None
- Metric
- User Preference (None)Note: This option has flexibility to apply the units of measure based on the selected system of measure of your preference. The value within the parentheses displays the system of measure you have selected or none if you have not selected anything. If you select a different system of measure as your preference the value will change accordingly.
The selections available in the System of Measure box populate when you select the options menu.
Procedure
What To Do Next
Load a Template Only After Selecting Template Options
About This Task
The selections available in the System of Measure box populate when you select the options menu.
Procedure
Select a Data Quality
You can select a time series data quality when you create a chart.
About This Task
When looking at chart data, you may want to view all the data or only the good quality data. Using this feature, when you create a Time Series Analysis or Event Data Analysis chart in the Analysis view, you can select the data quality filter for a view.
The options available in the Data Quality Filter box in Analysis views are based on the user preferences.
Data Quality Filter selection consists of:
- Show All Data
- Show Good Quality Data
- User Preference