Manage Alerts
About Alert Actions
In the alerts inbox and details page of an alert, you can perform various tasks.
- Claim and release an alert.
- Assign an alert.
- Assign a disposition to an alert.
- Add notes to an alert.
- Create an alert manually.
- Apply filters to an alert.
- Add evidence to an alert.
- Create and view a case from an alert.
- Create a recurring alert.
- Mark an alert as processed.
- Audit of an alert.
- Generate a PDF report for an alert.
- View an asset faceplate from an alert.
- View the analysis chart.
- View and add notes.
- View existing evidence and attach new evidence.
- View the audit results of an alert.
- View the list of linked cases with general visibility that are associated with the assets to which you have access.
- Export alerts to PDF.
Claim or Release an Alert
About This Task
- You cannot claim or release a claim for an alert that belongs to another tenant.
- When you release an alert, you automatically lose subscription to that alert.
Claiming an alert in the Ready state changes its status to In Process. If an alert is In Process, you cannot claim the alert until it has been released by the current owner.
Procedure
Assign an Alert
An analyst can assign an alert that belongs to the same tenant to another user.
Before You Begin
About This Task
Procedure
Results
Assign an Alert Disposition
After claiming an alert, you can assign a disposition to indicate its validity. Dispositions are retained when you release, process, or reclaim an alert.
About This Task
In the Alerts grid view, the default value for Disposition is None and the Disposition column is required. The Disposition column can be sorted as well.
Procedure
Add or Delete Notes in an Alert
Notes can help clarify evidence during a diagnosis.
About This Task
- Internal Notes
The INTERNAL NOTES section appears only if you have either View Internal Notes or Manage Internal Notes permission. If you have the View Internal Notes permission, you can view and read any internal notes, but cannot add or edit the note. The Manage Internal Notes permission allows you to view internal notes and add a note. However, you can delete only your own notes. The INTERNAL NOTES section can be viewed in the alerts grid.
- Notes
The NOTES section is available to all users with View Alert Detail or Manage Alert permission. If you have Manage Alert Detail permissions, you can edit or delete notes. The NOTES section appears in alerts grid as a column, and can be exported to a PDF.
Procedure
Add, Delete, or Download Evidence in an Alert
You can add files to an alert as evidence to help diagnose an issue. In addition, when you save an analysis of an alert in Analysis view, it appears as an evidence in the EVIDENCE section of the alert.
About This Task
- Image files (JPG, JPEG, PNG, BMP, TIF)
- Text type files (DOC, DOCX, XLS, XLSX, PPT, PPTX, TXT)
- PDF files
You cannot add folders or EXE, BAT, CMD, MSI, BIN, ZIP, RAR files as evidence.
You can download the files that are attached as evidence or delete the files that you have attached.
Procedure
Create an Alert Manually
You can create an alert at any level of the asset hierarchy that belongs to the same tenant.
Before You Begin
About This Task
You can create an alert to monitor potential issues. You can enter asset IDs at the enterprise, site, and segment levels, in addition to the actual asset.
Procedure
Results
Create Custom Filters for Alerts
You can create custom filters for alerts that have specific requirements.
About This Task
The default filter sets for alerts appear in the module navigation menu. By default, alerts are displayed in the alerts page based on the first filter set.
The filter sets allow you to view specific set of alerts by narrowing the entries. You can use the auto-refresh settings to display the newly added alerts. You can set the frequently used filters as favorites. When a new alert is added, the auto-refresh setting considers the existing filters and assigns the alert to the correct queue.
Procedure
Results

Apply Filters to Alerts
You can apply default or custom filter sets to Alerts.
About This Task
Procedure
About Recurring Alerts
You can create a reminder or recurring alerts for assets or tags that don't have any analytics running to generate alerts.
You can use the recurring alerts to review the current state of these assets for the given tags. The reminder criteria is time-based and shows the interval in minutes, as well as the event start time and event end time.
- Event start time – begins from the present time onwards.
- Event end time – is any date and time in the future.
You can create and schedule a recurring alert, cancel a scheduled recurring alert, and view recurring alerts in the alerts inbox and grid. An alert with indicates that it is a recurring alert.
Access a Recurring Alert
You can view recurring alerts in the Scheduled Alert Settings page.
Before You Begin
Procedure
Create a Recurring Alert
You can create a recurring alert in both the alerts inbox and alerts grid.
Before You Begin
About This Task
- You can create a recurring alert for an asset that belongs to the same tenant.
- You cannot create more than 2000 alerts in a series of recurring alert.
You can create a recurring alert in one of the following ways:
- From the Create an Alert window.
- From the Recurring Alerts page.
Procedure
Results
Create a Case from an Alert
To initiate and track the process used to address an issue identified in an alert, you can create a case from the corresponding details page of the alert.
Before You Begin
About This Task
You can create a case from an alert by providing an Asset ID at any level (enterprise, site, segment, or asset).
Procedure
Results
If you create multiple cases for a single alert, the Case Number in the Case Information section is incremented by one for each additional case.
Access a Case from an Alert
About This Task
When you create a case from an alert, the case is generated in the Cases module, and a link to the case appears in the LINKED CASES section in the details section or page of an alert.
Procedure
Link or Unlink a Case to an Alert
About This Task
- Case Name
- Case ID
- Asset ID
- Status
Procedure
Mark an Alert as Processed
About This Task
Procedure
Reopen a Processed Alert
After an alert has been processed, you cannot change its disposition state.
About This Task
After you reopen a processed alert, you can then use the same workflow as a new alert. The alert retains its previous case links and associated disposition state values. You can then create a case, or close the alert.
Procedure
Access Asset Faceplate from an Alert
The Asset Faceplate contains information about a selected asset, including equipment information, asset attributes, and associated tags.
About This Task
The Asset Faceplate is located in Assets, but you can view it in Alerts.
Procedure
Navigate to an External Link From an Alert
You can navigate to an external link from an alert if you have configured it in the associated alert template.
Procedure
View Asset Criticality for Alerts
You can view Asset Criticality for alerts in the Alerts Details page.
About This Task
Procedure
- In the module navigation menu, select .
- In the Alerts Details page, select the criticality number in the ALERT INFORMATION section to display the details of the criticality level in the Asset Criticality Analysis page in Predix Essentials.