Alerts Grid View
About Alert Grid View
By default, the alerts appear in tabular format. If you select to view alerts in the Inbox view, the selection persists, even if you log out and log in to the Predix Essentials application.


- 30 Sec
- 1 min
- 5 min
- 10 min
In the Alerts grid view, you can sort the grid columns by selecting the column header. Latched alerts will appear in the grid, and the COUNT column displays the number of times the specific alert has occurred, and the FIRST OCCURRENCE and LAST OCCURRENCE columns display the date and time when the alert occurred first and when it occurred last, respectively.
Column Header | Description |
---|---|
ALERT ID | The unique identification number for the alert. |
ALERT SOURCE | The source of the alert creation, such as Manual (creation), from SmartSignal, or from the Orchestration Manager. |
ALERT TYPE | The type of the alert. |
ALERT UUID | The universally unique identifier of the alert. |
ANALYSIS LINKS | The analysis views available for the alert. |
ANALYTIC INSTANCE | The SmartSignal analytic instance associated with the alert. |
ANALYTIC MODEL NAME | The contributing SmartSignal analytic model name. |
ASSET ALIAS | The alias for the asset name. |
ASSET CUSTOMER NAME | The name of the customer who owns the asset. |
ASSET CRITICALITY | The criticality of an asset along with the color. |
ASSET ID | The unique identification number of the asset that caused the alert. |
ASSET NAME | The name of the asset that caused the alert. |
ASSET PARENT | The parent asset of the asset associated with the alert. |
COUNT | The number of latch alerts for a grouped alert. If the alert is not latched, a dash (-) is displayed. |
DENSITY | The density value only appears for SmartSignal and SmartSignal Tag Rule alerts. For other types of alerts, the value is blank. |
DISPOSITION | The disposition of the alert, such as Valid or False. This column is required and the default value for an alert disposition is None. |
DISPOSITION QUALITY | The information on whether the disposition of an alert was correct or incorrect. This column contains a value only for the processed alerts. |
EVENT TIME | The date and time of the event occurrence that caused the alert. |
FIRST OCCURRENCE | The date and time of the first occurrence of the grouped alert. |
LAST OBSERVATION | The date and time of the last observation of the alert. |
LAST OCCURRENCE | The date and time of the latest occurrence of the grouped alert. |
LAST PROCESSED | The date and time of the last processing of the alert. |
LAST UPDATED | The date and time of the last update of the alert. |
LINKED CASES | The link to any linked cases attached to an alert, which opens the case in a separate browser tab. |
NAME | The name of the alert. |
NOTES | The number of notes present for an alert. Selecting the number opens a window where you can view the note details. You can filter the details by text. Note: Internal Notes are not viewable in grid view. |
OWNER | The name of the person who owns the alert. Note: In the following scenarios, the value that appears in the OWNER column is NULL:
|
RECEIVE TIME | The date and time when the alert was received. |
SEVERITY | The severity of the alert, where 1 being the most severe. |
SEVERITY CHANGE | The number of times the severity of the alert has been changed. |
SITE NAME | The name of the site where the asset is located. |
SOURCE KEY | The source key of the asset. |
STATUS | The status of the alert such as Ready (to be claimed), In Process (alert has an owner), or Processed (alert has been marked as processed). |
TENANT ID | The unique identification number of the tenant associated with the alert. |
USER NAME | The name of the person who claimed the alert. When an alert is unclaimed, the value for User Name is NULL. |
VISIBILITY | The visibility of an alert, for example, Limited or General. You can view the alerts with Limited visibility if you have the Limited visibility permissions. Anyone with permissions to view alerts can view the alerts with General visibility. You can filter and sort this column in the grid. You can change the visibility by selecting the Name of the alert. You must refresh the screen for the change to take effect. |
If you select a column header, the grid is primarily sorted for the selected column alphabetically in ascending or descending order, and secondarily sorted by Alert Time Received (latest on top).
In the Alert Inbox grid view, if you select a different filtered Alert inbox in the module navigation menu or apply a new filter set using More Filters, the new filtered inbox appears in the grid view.
Selecting an alert displays the Alert Details page in another tab.
Toggle the Alert Inbox View
You can switch between the Alerts Inbox and Alerts Grid anytime while viewing the alerts.
About This Task
Procedure
Access Alerts of an Asset in Alerts Grid
The Asset Hierarchy section in an alerts grid provides you with an option to select an asset such that you can view the alerts related to the asset. You can select multiple assets and the alerts associated with the selected assets appear in the alerts grid.
About This Task
Procedure
Results

You can apply your favorite filters to the list of alerts.
The selection, and the open or collapsed state of the hierarchy persists, and it is available the next time you access the application.
Add and Remove Columns in the Alerts Grid
You can show or hide certain columns in the Alerts Inbox grid view.
About This Task
Use the columns drop-down list box to add and remove columns in the Alert Inbox grid view.
Procedure
- To add a column using the Show Columns drop-down list box:
- To add a column using the Table Settings window:
- To remove a column using the Show Columns drop-down list box:
- To remove a column using the Table Settings window:
Sort and Filter Columns
Sorting and filtering columns allow you to categorize and find the required data easily.
Before You Begin
- View Alert Detail
- View Limited Visibility Alerts
- Alerts
- Manage Alerts
About This Task
Procedure
- To sort a column:
- To filter a column:
Reorder Columns in Alerts Grid
You can customize the alerts grid by reordering the columns.
Before You Begin
About This Task
- Change alerts
- Navigate away from the Alerts module
- Change the alert filter set
- Log out and then log back in
Procedure
- To reorder the columns by dragging:
- To reorder the columns using the Table Settings window:
Freeze Columns in Alerts Grid
About This Task
Procedure
Group Columns
Grouping of columns organizes data in different levels.
Before You Begin
- You can group the following columns:
- ALERT SOURCE
- ASSET ALIAS
- ASSET CUSTOMER NAME
- ASSET ID
- ASSET NAME
- ASSET PARENT
- DISPOSITION
- OWNER
- SEVERITY
- SITE NAME
- STATUS
- USER NAME
Procedure
Results
- For uninterrupted performance, while an operation is being performed on grouped columns, do not perform another operation at the same time. We recommend that you wait for the operation to complete.
- In Internet Explorer, to filter data in the grid, double-click the Filter box, and then enter the text.
View Linked Cases in Alerts Grid
You can view the case details associated with an alert by selecting the linked cases in the alerts grid.
Before You Begin
About This Task
Procedure
View Notes in Alerts Grid
About This Task
Procedure
Generate a PDF Report for an Alert
Before You Begin
- Alerts
- View Alert Details
- Manage Alerts
About This Task
- ASSET INFORMATION
- ANALYSIS
- SCAN GROUP DATA
- NOTES
- EVIDENCE
- LINKED CASES
- If an analysis or evidence of an alert contains multiple cards, only the charts of the first card appear in the generated PDF report.
- A generated PDF report for an alert can contain up to eight charts of an analysis or evidence.
Procedure
Results
Select Alerts for Bulk Action
Before You Begin
About This Task
Procedure
Access the SmartSignal Analytic for Maintenance from the Alerts Grid
Performing maintenance is the process of selecting an analytic instance associated with an alert for maintenance and retraining the analytic instance if it generated a spurious alert because the analytic instance did not accurately reflect the current operating state. You can access the analytic instance associated with a SmartSignal alert from the ANALYTIC INSTANCE column in the alerts grid.
Before You Begin
- The Alerts or Manage Alerts permission to change the status of the alert to In Process Maintenance. Note: You can change the status of an alert other than SmartSignal alerts to In Process Maintenance. However, you cannot access the analytic instance for the alert.
- The SmartSignal Mapping permission to modify an analytic instance of a SmartSignal alert. For more information on SmartSignal permissions, refer to Default Permission Set Definitions in the Users and Permissions documentation.