Overview

Overview of the Alert Templates Module

When you create and deploy an analytic, you can use free-form text to associate the analytic with one or more alert templates.

Multiple analytics can be associated with a single alert template. When an analytic triggers an alert, the system checks for associated alert templates, which it uses to route alerts to the correct inbox. You can use alert templates to facilitate the ingestion of alerts into Predix Essentials.

When you create an analysis view, it is associated with an asset or an asset class. These new views can be added to an alert template. This allows you to customize alert analysis views for specific alert types.

Alert templates connect and automate alerts received from sensors by providing the following information:
  • Assigned data severity.
  • One or more assigned analysis views.
  • Analytic source.
  • Alert issue type.
Tip: You need specific permissions to complete these tasks. For more information on the permission sets, refer to the Users and Permissions documentation.
The following definitions are helpful when selecting options for an alert template:
Consumable
Toggle for allowing alerts to appear in the alert inbox. Default is on.
Trip
Toggle for designating associated alerts as trip alerts that require immediate action. Default is off.
Severity
The importance assigned to an alert when triggered by a predictive analytic.
Type
The type of alert being used, such as vibration or combustion.
Source
The pool of predictive analytics used to display anomalous data received from asset sensors.
Active
Toggle to indicate that the template is active. Alerts can be ingested by an analytic or created manually only when the alert template is active.
External Links
A way to add external links to an alert template so they can be viewed in a new page from an associated alert.
Case Templates
A way to associate a case template with an alert template.
Analysis View (Templates)
Rules associated with building views for an alert.