Text Display
Use this plug-in to add display-only text in your application.
The widget is available under designing application pages, drag-and-drop Text Display to a container. To use the old version, refer to Text.
. WhenText Properties
Field Name | Description |
---|---|
Source > Label | Provide the input data source to receive label names for the text plugin. |
Source > Input Value | Provide the input data source to receive values for the text plugin. |
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. The decimals will apply to Input Value, Minimum Value, and Maximum Value properties. |
Label Styling | Formats the label: Font Family, Font Size, and Font Color formats the text. |
Hidden | Select this check box if you want to hide the
plug-in. To show the hidden plug-in in Operations Hub new layout, go
to Page Visuals and under
Action column, select ![]() |