Pivot Grid
Pivot grid allows to visualize data in a multi-dimensional format.
- Rename rows/columns to replace lengthy tag names
- Apply conditional formatting to rows/columns based on values
- Calculate values quickly using totals
- Sort, filter, and summarize data
- Export pivot data to Excel
The pivot grid is available under designing application pages, drag-and-drop GEPivotGrid to a container.
. WhenThe following list of properties are specific to this widget. For common properties, refer to Page Components (Classic).
Pivot Grid Properties
Field Name | Description |
---|---|
Source - Input | To enable the pivot grid, provide values from a data source.
|
Use Raw Format | Select the check box to display numbers in raw format. For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off. |
Number of decimals | This option appears if you do not want to display numbers in raw
format. In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number. The decimals will apply to all the pivot grid columns that contain numeric values. |
Height (px) - 0 equals dynamic | Set a height for the pivot grid in pixels. If set to 0, the widget occupies 100% of its container. |
Row Header Width (px) - 0 equals dynamic | Set a width for the header row in pixels. |
Show Borders | Select the check box to apply a border to the pivot grid table. To remove the border, clear the check box. |
Allow Sorting | Select the check box to sort the rows and columns alphabetically by default. |
Allow Sorting by Summary | Select the check box to provide an option to sort the rows by
column. At runtime, right-click the column you want to sort by and select the sorting option. |
Allow Filtering Row/Column Values | Select the check box to provide an option to filter data at runtime. |
Allow Expand/Collapse All | Select the check box to enable expand/collapse data levels at
runtime. Your pivot grid should have multiple data levels to use this property. For value-based table cell data, you can expand and collapse data details to aggregate values. |
Allow Export | Select the check box to allow exporting data at runtime. |
Show Row Totals | Select the check box to show totals for each row. |
Show Row Grand Totals | Select the check box to show the grand totals for each row. |
Show Column Totals | Select the check box to show totals for each column. |
Show Column Grand Totals | Select the check box to show the grand totals for each column. |
Field Configuration | Configure pivot grid rows, columns, and data. Map all the three
areas (rows, columns, data).
|
Field Name | Description |
---|---|
Cell Color | Select a color for the pivot grid table cells. |
Cell Font Color | Select a font color for the pivot grid table cell text. |
Column Header Font Color | Select a font color for the pivot grid table column header text. This helps to differentiate the header text from the cell text. |
Totals Background Color | Select a unique cell color for the row/column totals. |
Totals Font Color | Select a font color for the row/column totals text. |
Hidden | Select this check box if you want to hide the
plug-in. To show the hidden plug-in in Operations Hub new layout, go
to Page Visuals and under
Action column, select ![]() |
Field Name | Description |
---|---|
Item Display |
|
Conditional Formatting | Apply conditions to format cells based on values. You can create
more than one condition for a Row/Column Value.
The conditions are applied according to their order of display. If more
than one rule matches a particular cell, the first condition in the list
to match takes effect and rule processing for that cell will
stop. Select +Add Item for options to
create conditions. For example, format a cell if its value is less
than 9000:
Tip: If you want to format a row/column with a
color that does not change based on value, apply the
Always comparison
operator. |
Pivot Grid at Runtime



- You can switch the position of row and column fields. To switch a field position, drag and drop the field in the desired row/column.
- You can apply multiple filters to the data to get focused results.
- You can sort fields by ascending/descending order.

- Under All Fields, clear the check box for
Name
. The field is removed from Row Fields. - Under All Fields, select the check box again for
Name
.The
Name
field may not show up under Row Fields. It may show up under column or data fields. In such cases, drag and drop the field to the appropriate location.