Set up CIMPLICITY Project User Security

To avoid having to login on the Webspace container to the project, for each user that is configured in Operations Hub, a matching user must be configured in the CIMPLICITY project.

Procedure

  1. Open the CIMPLICITY Project in the CIMPLICITY Workbench.
  2. Go to Security > Users.
  3. For each user in the Operations Hub configuration, create a CIMPLICITY user of the same name with a security type of CIMPLICITY.
    Note: The passwords for the user between Operations Hub and the CIMPLICITY project do not need to match.