Upgrade Operations Hub
This topic describes the steps to upgrade the application.
Before you begin
Close any applications or components before upgrading Operations Hub.
About this task
- First uninstall the existing version on your system, and then install the new version. Uninstallation allows to purge the database. (OR)
- Directly install/upgrade the new version without uninstalling the existing version. No scope for purging the database.
Procedure
- Uninstall the existing version of Operations Hub if you want to purge the database.
- Install the newer or the latest version of Operations Hub.
- Restart your computer following an upgrade of Operations Hub if Plant Applications and Operations Hub coexist on the same resource.
-
On upgrading to Operations Hub 2022 or
later, the IQP designer uses
app_name
instead ofapp_id
in its URLs. -
If upgrading from 2.0 to 2.1 or later, restart the WebClient services to allow the
Plant Applications Web Client to connect successfully to Operations Hub.
- If using Enterprise WebClient version, restart the Docker service.
- If using Standard WebClient version, restart the GE PlantApps WebClient Master Control service.
- If you have installed Operations Hub 2022 or 2022 SP1, restart your machine prior to WebClient installation.
- Remember to clear your browser cache after upgrading to a newer version of Operations Hub.
-
If a firewall is running on the server, configure the firewall to make sure the
public https port used by Operations Hub Public is not blocked. Typically, the port
is
443
, but can be a different value that you have selected or that was changed to avoid a conflict. If you are not sure of the port number, the shortcut (URL) placed on the desktop should contain it.