Have You Seen Operations Hub Lately?Click here to check out all the new features in the latest version.
Supercharge your Proficy solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy here.
Uninstall Operations Hub on Windows
Procedure
If you want to uninstall Operations Hub automatically, open Command Prompt, and enter the following command: <Installation folder path of Operations Hub>\OpHub-Windows_Installer>ophub_bundle -uninstall
If you want to uninstall Operations Hub
manually, perform the following steps:
On the machine on which you want to uninstall Operations Hub, select Control Panel > Uninstall a Program.
A list of programs that you can uninstall appears.
Right-click Operations Hub, and then select
Uninstall.
The Uninstall Options page
appears.
In addition to uninstalling Operations Hub, if you want to
delete all the related data and applications, select the
Purge databases during uninstall check
box.
Select Next.
The You are ready to uninstall page appears.
Select Uninstall.
Results
Operations Hub is uninstalled from the Windows machine.