Map Existing UAA Groups With Proficy UAA
About this task
Procedure
-
Double-click
.
Tip: By default, this icon appears on the desktop after you install Proficy UAA. -
Select the Identity Providers tab.
The UAA/LDAP/SAML Connectivity Tool appears.
- Select the Map Existing UAA Groups check box.
- In the UAA Connection section, provide values as specified in the following table.Important: The values that you provide in this step must match the values that you provided in the while installing your Proficy product. These values are required to connect to Proficy UAA.
Box Description URL Enter the authorization server URL of the Proficy UAA server that you specified in the UAA Base URL box during installation (for example, https://localhost). If referencing Historian 7.x UAA, then use a url of https://Historian7x:8443; if referencing Historian 8.x then use a URL of https://Historian8x (no port number). The port numbers reflect the default port numbers for Historian. If ports were customized, then use the selected port.
Client ID Enter the client ID of the Proficy UAA server that you specified in the Admin Client ID box during installation. Client Secret Enter the client secret configured for the OAuth client that you specified in the Admin Client Secret box during installation. - Select Test.If connection to the UAA server is established, a message appears, confirming the same.
- Select Continue.In the UAA Mapping section, the drop-down list box contains a list of groups in Proficy UAA. In the Filter box, a list of groups in the existing UAA instance appear.
- In the drop-down list box, select the Proficy UAA group to which you want to map the existing UAA groups.
- In the Filter box, select the check boxes corresponding to the existing UAA groups that you want to map. Note: If a group is already mapped to the Proficy UAA group that you have selected, the check box is already selected.Tip: Clear the check boxes corresponding to the UAA groups for which you want to remove the mappings.
- Select Map Members.A message appears, confirming that the Proficy UAA group is mapped to the existing UAA groups that you have selected.
- Repeat steps 7 through 9 for all the Proficy UAA groups that you want to map.