Pages and Windows
The Data Quality Parameters Window
- Error Event Percentage: The percentage of Events that contain an error, as a function of the total Events.
For example, if there are 100 Events out of which 20 have an error, the Error Event Percentage is 20%.
This data provides information about how many Events that are used for reporting contains errors.
- Total Report Time: The duration for which you are importing the Events, in minutes.
- IU Time Percentage: The percentage of the total IU time for the Events, as a function of the total report time.
For example, if the total report time is 100 minutes, and the sum duration of the IU Events is 20 minutes, the IU Time Percentage is 20%.
- Aggregated Error Code: The two-digit bit-mapped code that indicates the result of the validation performed on the Sub Group. The left bit indicates whether at least one Event existed for each wind turbine per hour. The right bit indicates whether the sum duration of the Events is same as the total report time for the Sub Group. The value 0 in either location indicates that the validation passed, whereas the value 1 indicates that it failed.
- Total Events: The total number of Events.
- Total Error Events: The total number of Events that contain an error.
- Error Time Percentage: The percentage of the total error time for the Events, as a function of the total report time.
For example, if the total report time is 100 minutes, and the sum duration of Events that have an error is 20 minutes, the Error Time Percentage is 20%.
- Total IU Time: The sum duration of the IU Events (that is, Events that have the value IU in the IEC Event Type field), in minutes.
- Total Error Time: The sum duration of Events that have an error, in minutes.
- IU Event Percentage: The percentage of the IU Events, as a function of the total Events.
For example, if there are 100 Events out of which 20 have the value IU in the IEC Event Type field, the IU Event Percentage is 20%.
The Events Workspace and the GAA Wind Edit Events Page
- The Events workspace, which appears in the Sub Group Summary page with a table of Events.
- The GAA Wind Edit Events page, which appears when you select Edit Events in the All Events section in the GAA Wind Overview page.
Task | Location | Description |
---|---|---|
Filter the Events based on the period and history. | The Events workspace. |
Select , and then, in the Filter By Date Range window, modify the values in the following boxes as needed:
Important: When filtering Events, the values in the From and To boxes are treated as Coordinated Universal Time (UTC) values to ensure accuracy in the count of Events retrieved for a given period, regardless of your time zone. Note:
|
Modify the count of Events that appear in the table in a given page. | The Events workspace and the GAA Wind Edit Events page. |
Select one of the following buttons:
|
Sort the Events in ascending or descending order based on one or more columns. | The Events workspace and the GAA Wind Edit Events page. |
Right-click the column heading, and then select Sort Ascending or Sort Descending as needed. |
Clear the sorting in the columns. | The Events workspace and the GAA Wind Edit Events page. | Right-click the column heading, and then select Clear Sorting. |
Display or hide the columns. | The Events workspace. |
When you select , the Column Chooser window appears, where all the columns appear with check boxes. By default, these check boxes are selected, indicating that the corresponding columns appear in the table. To hide a column in the table, clear the check box next to the column. |
Display or hide the columns. | The GAA Wind Edit Events page. |
When you select , the Column Chooser window appears, where all the columns appear with check boxes. By default, these check boxes are selected, indicating that the corresponding columns appear in the table. To hide a column in the table, clear the check box next to the column. |
Group the Events by one or more columns. | The Events workspace and the GAA Wind Edit Events page. |
Right-click the column heading, and then select the Group by this column option. Alternatively, you can drag the column heading next to , where the following text appears: Drag a column heading here to group by that column.
Note: The order in which these column headings appear in the table when you group the Events corresponds to the order in which they appear next to . You can modify the order next to by dragging the column headings to where you want them. |
Ungroup the Events by one or more columns. | The Events workspace and the GAA Wind Edit Events page. |
Right-click the column heading next to or in the table, and then select the Ungroup option.
Tip: To ungroup the Events by all columns at once, right-click a column, and then select the Ungroup All option. |
Filter the Events using the column headings. | The Events workspace and the GAA Wind Edit Events page. |
When you select next to any column heading except NERC State, a list of values that are available in the column appears with check boxes; for the NERC State column heading, a list of all NERC states appears with check boxes.
Note: does not appear for the Start Date and End Date columns. Select the check boxes next to the values based on which you want to filter the Events, and then select OK.
Tip: To select all the check boxes at once, select the Select All check box, and then select OK. To remove certain values from the filter, clear the check boxes next to those values, and then select OK.
Tip: If all the check boxes were previously selected and you want to now clear all the check boxes at once, clear the Select All check box, and then select OK. |
Filter the Events using regular expressions. | The Events workspace and the GAA Wind Edit Events page. |
Point to below a column heading, and then select one the following options as needed:
|
Filter the Events using the column values. | The Events workspace and the GAA Wind Edit Events page. |
For a column that contains check boxes, select in the drop-down list box below the column heading, and then select one of the following options as needed:
To apply the filter, select . For the Start Date and End Date columns, select in the drop-down list box below the column heading. In the calendar that appears, modify the date and time as needed, and then select Done. To apply the filter, select . For a column that does not contain check boxes, enter the value (that is, the filter criterion) in the text box below the column heading, and then select .
Note: In the text box, the Events are filtered using the Contains regular expression. Therefore, you can enter a partial value in the text box. |
Clear, at once, all the filters applied using the column headings, regular expressions, and column values. | The Events workspace and the GAA Wind Edit Events page. |
Select Clear Filter. |
Bulk Edit | The Events workspace and the GAA Wind Edit Events page. | Select , and then select the check boxes next to the fields whose values you want to modify. After modifying the values, select Update. In the GAA Wind Edit Events page, the cells whose values you have modified are highlighted. |
Create Events | The Events workspace. | For more information, refer to the Create Events section of the documentation. |
Split an Event | The Events workspace and the GAA Wind Edit Events page. | For more information, refer to the Split an Event section of the documentation. |
Discard Changes | The Events workspace and the GAA Wind Edit Events page. | Select to discard your changes. |
Export Events | The Events workspace. | For more information, refer to the Export Events section of the documentation. |
The Error Code Window
- The All Events and Edited Events sections in the GAA Wind Overview page.
- The GAA Wind Edit Events page.
- The Events workspace in the Sub Group Summary page.
Position of 1 | Error Name | Error Message Description |
---|---|---|
First | Error 1 | The end time stamp of the Event does not equal the start time stamp of the next Event. |
Second | Error 2 | The start or end time stamp of the Event does not fall within the requested period of the API call. |
Third | Error 3 | Information is unavailable. |
Fourth | Error 4 | The production value of the Event is out of range for the associated Sub Group. |
Fifth | Error 5 | Warning: The Event falls within the recommended coverage delay period. |
Sixth | Error 6 | The production value of the Event exceeds the maximum production value for the associated Sub Group. |