Fuel Types

Access a Fuel Type

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes section, select Fuel Types.

    The Fuel Types subsection appears, displaying the following columns of information:

    • Fuel Code
    • Fuel Description
    • Regulatory Organization
    • Mapped ID

  3. Locate the row that contains the Fuel Code that you want to access.
  4. In the Fuel Code column, select the link.

    The Edit Fuel Type window appears, displaying the datasheet for the selected Fuel Code.

    Note: As needed, you can modify the values in the available fields, and then select to save your changes.

Add a Fuel Type

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes section, select Fuel Types.

    The Fuel Types subsection appears.

  3. In the upper-left corner of the Fuel Types section, select .

    The Add Fuel Type window appears.

  4. As needed, enter the values in the available fields.
  5. Select .

    The new Fuel type is added.

Delete a Fuel Type

About This Task

Important: You must not delete a baseline Fuel Type.

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes section, select Fuel Types.

    The Fuel Types subsection appears.

  3. Select the row containing the Fuel Type that you want to delete.
  4. In the upper-right corner of the Fuel Types section, select .

    The Delete Fuel Type dialog box appears, asking you to confirm that you want to delete the selected Fuel Type.

  5. Select Yes.

    The selected Fuel Type is deleted and the updated list of Fuel Types appears.