Amplification Codes

Access an Amplification Code

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes section, select Amplification Codes.

    The Amplification Codes subsection appears, displaying the following columns of information:

    • Amplification Code
    • Code Description
    • Unit Type
    • Event Type
    • Regulatory Organization

  3. Locate the row that contains the Amplification Code that you want to access.
  4. In the Amplification Code column, select the link.

    The Edit Amplification Code window appears, displaying the datasheet of the selected Amplification Code.

    Note: As needed, you can modify the values in the available fields, and then select to save your changes.

Add an Amplification Code

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes subsection, select Amplification Codes.

    The Amplification Codes section appears.

  3. In the upper-left corner of the Amplification Codes section, select .

    The Add Amplification Code window appears.

  4. As needed, enter the values in the available fields.
  5. Select .

    The new Amplification Code is added.

Delete an Amplification Code

About This Task

Important: You must not delete a baseline Amplification Code.

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes subsection, select Amplification Codes.

    The Amplification Codes section appears.

  3. Select the row containing the Amplification Code that you want to delete.
  4. In the upper-right corner of the Amplification Codes section, select .

    The Delete Amplification Code dialog box appears, asking you to confirm that you want to delete the selected Event Type.

  5. Select Yes.

    The selected Amplification Code is deleted and the updated list of Amplification Codes appears.