Event Types

Access an Event Type

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes section, select Event Types.

    The Event Types subsection appears, displaying the following columns of information:

    • Event Type Code
    • Event Type Description
    • Color Code
    • Mapped ID
    • Regulatory Organization

  3. Locate the row that contains the Event Type that you want to access.
  4. In the Event Type Code column, select the link.

    The Edit Event Types window appears, displaying the datasheet of the selected Event Type.

    Note: As needed, you can modify the values in the available fields, and then select to save your changes.

Add an Event Type

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes section, select Event Types.

    The Event Types subsection appears.

  3. In the upper-left corner of the Events Types section, select .

    The Add Event Type window appears.

  4. As needed, enter the values in the available fields.
  5. Select .

    The new Event Type is added.

Delete an Event Type

About This Task

Important: You must not delete a baseline Event Type.

Procedure

  1. Access the GAA Administrator page.
  2. In the System Codes section, select Event Types.

    The Event Types subsection appears.

  3. Select the row containing the Event Type that you want to delete.
  4. In the upper-right corner of the Events Types section, select .

    The Delete Event Type dialog box appears, asking you to confirm that you want to delete the selected Event Type.

  5. Select Yes.

    The selected Event Type is deleted and the updated list of Event Types appears.