Admin
Overview of the Root Cause Analysis (RCA) Module
The APM Root Cause Analysis (RCA) module lets you conduct a root cause analysis, which allows you to analyze causes of failures. A Root Cause Analysis also allows you to track the performance of the equipment by following implementation of recommendations. When you create a Root Cause Analysis, you are using APM tools to facilitate a standard process that is based on the PROACT® for Meridium methodology.
More Details
A root cause analysis is the process of analyzing failures down to their root causes, which can include but is not limited to physical causes, human causes, and latent causes of the failure.
In the APM system, elements of a Root Cause analysis store all the information necessary for the team to identify a root cause for failure of and asset.
When the Root Cause Analysis is complete, it can be published and made available to users who are not members of the analysis team, allowing them to view the results using APM tools.
When a failure occurs in your facility, there could be any number of causes that led to the failure. If you investigate the causes, you might find that each failure is caused by another higher-level cause. If this root cause remains unidentified, the failures will likely persist.
For instance, consider an example of a car that has had trouble starting every month for the past three months. In this case, you might determine that:
- In the first month, the cold weather caused the failure.
- In the second month, the battery was low.
- In the third month, the warning to check engine was displayed in the dashboard.
If you were to conduct a root cause analysis on the car, you may find that while each month's failure had its own apparent cause, the root cause of each failure was that a voltage regulator was malfunctioning.
To help you identify the root causes of failures in your facility, you can assemble an RCA Team that will:
- Collect data relevant to the failure.
- Analyze the data.
- Develop hypotheses about the root cause.
- Develop recommendations for preventing the failure from occurring or lessen the impact of the failure in the future.
- Implement recommended solutions.
- Track implemented solutions and re-evaluate them, as needed.
Access the RCA Administrator Page
About This Task
To access the RCA Administrator page, you must be a Super User or a member of the MI PROACT Administrator Security Group.
Procedure
The RCA Administrator page appears, displaying the following tabs:
- Team Charter: Contains the default Team Charter. You can specify the Team Charter that will appear when you access the Team Charter section for an RCA.
- Critical Success Factors: Contains a list of the Critical Success Factors (CSFs) that will appear by default in the Available CSF section when you access a CSF for an RCA.
- Default Settings: Contains the following settings:
- Queries: Contains the Catalog path to the Tracking Evaluation Query that is provided in the baseline APM database.
- Logic Tree Auto-Arrange: Allows you to determine whether or not the nodes on a Logic Tree can be repositioned.
- Recommended Status and State: Allows you to select how the state of a recommendation is determined.
- Restricted Access: Allows you to decide whether or not access is restricted.
- Email Settings: Contains the alert settings for State Management emails.
- Event Color Settings: Contains color mappings for events on the Event Timeline.
- RCA Pages Setting: Contains a selections for the diagram and process pages that appear in the RCA module.

Modify the Default Team Charter
Procedure
Results
After you modify the default Team Charter, your changes will appear in:
- The Team Charter workspace on the RCA Administrator page.
- The Team Charter section in the Analysis Summary workspace, if you use the default Team Charter in an RCA.
Create a New Default Critical Success Factor
About This Task
Procedure
Results
After you create a default Critical Success Factor, it appears in:
- The Default Critical Success Factors list in the Critical Success Factors workspace on the RCA Administrator page.
- The Available CSFs list in the Analysis Summary workspace, when you try to create a new Critical Success Factor.
Modify a Default Critical Success Factor
About This Task
Procedure
Results
- The Default Critical Success Factors list in the Critical Success Factors workspace on the RCA Administrator page.
- The Available CSFs list in the Analysis Summary workspace, when you try to create a new Critical Success Factor.
Delete a Default Critical Success Factor
About This Task
Procedure
Results
When you delete a default Critical Success Factor, it will be removed from:
- The Default Critical Success Factors list in the Critical Success Factors workspace on the RCA Administrator page.
- The Available CSFs list in the Analysis Summary workspace, when you try to create a new Critical Success Factor.
Specify the Tracking Evaluation Query
About This Task
Procedure
Specify Logic Tree Auto-Arrange
Procedure
Configure State Management Email
Procedure
Add an Event Color or Icon Setting
You can select map specific colors or icons to appear for different event types in the Event Timeline. After mapping a color or icon to an event type, any Event records of that type appear in the Event Timeline in the selected color or icon.
Procedure
Modify an Event Color or Icon Setting
Procedure
Delete Event Color Settings
Procedure
Configure RCA Pages Setting
You can configure which diagrams and processes appear by default within the RCA module.