Manage Translations Upgrade
Upgrade or Update Manage Translations to V5.1.2.0.0
The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.
Upgrade from | Upgrade to | Procedure |
---|---|---|
V5.1.x | V5.1.2.0.0 | |
V5.0.x | V5.1.2.0.0 | |
V4.6.2 or a later V4.6.x release | V5.1.2.0.0 |
Upgrade from any version V5.1.0.0.0 through V5.1.1.0.0
This module will be upgraded to V5.1.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.
Upgrade from any version V5.0.1.0.0 through V5.0.4.0.0
The following tables outline the steps that you must complete to upgrade this module to V5.1.2.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Note |
---|---|---|
1 | Run the Meridium.Localization.EnableTranslations.exe file located in the following folder: C:\Program Files\Meridium\ApplicationServer\localizer\EnableTranslation\ | This step is required to update the translation content being delivered. |
Upgrade from any version V4.6.2.0.0 through V4.6.8.0.0
The following tables outline the steps that you must complete to upgrade this module to V5.1.2.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes |
---|---|---|
1 | Import translations. | This step is required only if you have previously customized translations for UI or metadata strings. |
Import Translations
About This Task
Procedure
- Export translations from a previous version:
- Import translations into the latest version: