Asset Strategy Management Upgrade
Upgrade or Update ASM to V5.1.2.0.0
The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.
Upgrade from | Upgrade to | Procedure |
---|---|---|
V5.1.x | V5.1.2.0.0 | |
V5.0.x | V5.1.2.0.0 | |
V4.6.2 or a later V4.6.x release | V5.1.2.0.0 | |
V4.6.1.x or earlier | V5.1.2.0.0 |
Note: For more information on upgrading to APM V4.6.2.0.0 or a later V4.6.x release, refer to the Upgrade documentation for the corresponding version.
|
Upgrade from any version V5.1.0.0.0 through V5.1.1.0.0
Action field mappings for Inspection, Calibration, and Proof Test Tasks have been converted from business rules to Policies, as a result any rules-based customization of these mappings will need to be manually implemented using the new mapping Policies via the Action Mapping workspace within the ASM Admin page.
Upgrade from any version V5.0.1.0.0 through V5.0.4.0.0
Action field mappings for Inspection, Calibration, and Proof Test Tasks have been converted from business rules to Policies, as a result any rules-based customization of these mappings will need to be manually implemented using the new mapping Policies via the Action Mapping workspace within the ASM Admin page.
Upgrade from any version V4.6.2.0.0 through V4.6.8.0.0
Action field mappings for Inspection, Calibration, and Proof Test Tasks have been converted from business rules to Policies, as a result any rules-based customization of these mappings will need to be manually implemented using the new mapping Policies via the Action Mapping workspace within the ASM Admin page.