Asset Strategy Implementation Upgrade

Upgrade or Update Asset Strategy Implementation (ASI) to V5.1.2.0.0

The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.

Upgrade from Upgrade to Procedure
V5.1.xV5.1.2.0.0
V5.0.xV5.1.2.0.0
V4.6.2 or a later V4.6.x releaseV5.1.2.0.0
  1. Upgrade from any version V4.6.2.0.0 through V4.6.8.0.0
  2. Upgrade from any version V5.0.1.0.0 through V5.0.4.0.0
V4.6.1.x or earlierV5.1.2.0.0
  1. Upgrade from any version V4.6.1.x or earlier to V4.6.2.0.0 or a later V4.6.x release
  2. Upgrade from any version V4.6.2.0.0 through V4.6.8.0.0
  3. Upgrade from any version V5.0.1.0.0 through V5.0.4.0.0
Note: For more information on upgrading to APM V4.6.2.0.0 or a later V4.6.x release, refer to the Upgrade documentation for the corresponding version.

Upgrade from any version V5.1.0.0.0 through V5.1.1.0.0

This module will be upgraded to V5.1.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.

Upgrade from any version V5.0.1.0.0 through V5.0.4.0.0

The following tables outline the steps that you must complete to upgrade this module to V5.1.2.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

StepTaskNotes
1As applicable, reconfigure any rule-based customization for the following items:
  • Action Mappings
  • Executing Mappings
  • Definition Configuration
  • Import from SAP
  • Export to SAP
This step is required only if you created rule-based customization in a previous version of APM. To support Asset Strategy Implementation (ASI) on cloud, rule-based customizations will no longer be valid (except the customizations for Package Builder, PRT Report Builder, and Object List Items Import). If you created rule-based customization in a previous version of APM, you must reconfigure them using the Asset Strategy Implementation Admin page.

Upgrade from any version V4.6.2.0.0 through V4.6.8.0.0

The following tables outline the steps that you must complete to upgrade this module to V5.1.2.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

StepTaskNotes
1Upgrade the ASI for SAP ABAP add-on in your SAP System.This step is required.
2As applicable, reconfigure any rule-based customization for the following items:
  • Action Mappings
  • Executing Mappings
  • Definition Configuration
  • Import from SAP
  • Export to SAP
This step is required only if you created rule-based customization in a previous version of APM. To support Asset Strategy Implementation (ASI) on cloud, rule-based customizations will no longer be valid (except the customizations for Package Builder, PRT Report Builder, and Object List Items Import). If you created rule-based customization in a previous version of APM, you must reconfigure them using the Asset Strategy Implementation Admin page.