System Requirements
System Requirements
An Atom must be installed within your network to connect to source systems and process the data into APM applications hosted on On-premise APM . The Atom will process and transmit data within your network boundary.
Supported Operating Systems
Operating system | Version |
---|---|
Windows 64-bit | APM Connect supports Windows Server 2016, 2019, or 2022 |
Hardware Requirements
The requirements for a single Atom that must process high volumes of data are:
Processor |
Dual 64-bit processors or higher (with 8 or 16 Cores) More processors allow for increased, simultaneous process runs |
Memory |
32 GB of RAM (minimum 8 GB dedicated to the Atom) More RAM allows for increased, simultaneous process runs |
Hard disk | 100–200 GB of hard disk space |
Java Runtime
Java (for Windows and Linux) | Java 8 or 11 (Preferred) |
---|---|
Java runtime (for Windows and Linux) |
Support for the following Java Runtime Variants:
Note: It is recommended to use the Java distribution from the remote management platform so that Java updates can be managed remotely (including automation). |
Java Information Panel |
Boomi provides a view to Java in use by the Atom in the management view.
|
Software Requirements
- Postgres (included as part of the installer for southbound services)
- SAP Integration
- Install sapnwrfc (an open-source library) for .Net Core framework to connect to SAP. (https://github.com/huysentruitw/SapNwRfc)
- The above open-source library requires the SAP NetWeaver RFC Library 7.50 SDK C++ binaries be installed locally. (SAP LaunchPad Download Link: the SAP NetWeaver RFC Library 7.50 SDK C++ )
- In addition to the installation, the .dlls and .lib files (icudt50.dll, icuin50.dll, icuuc50.dll, libsapucum.dll, libsapucum.lib, sapnwrfc.dll, sapnwrfc.lib) need to be copied to the southbound service installation folders
-
- *sapjco3.jar and sapjco.dll specific to the customer sap version are available in the below directories:
- C:\windows\system32
- {atom_name}/userlib directory
- *sapjco3.jar and sapjco.dll specific to the customer sap version are available in the below directories:
- Install the 64-bit version of the Visual C++ 2013 Redistributable package (Microsoft Download Link)
- Add Postgres 42.5.4 jar (Postgres JDBC Download Link) to {atom_name}/userlib directory
Required Service Ports
To provide communication between APM Connect server and other systems, make sure the listed ports are open.
Port Numbers | Description |
---|---|
5013/8040 (Ingress for the Service) | The service can listen on any port as per its configuration. It is recommended to use a unique port that would not interfere with other standard applications running on the server where it is hosted. |
80, 9080, 8879, 9043, 9044, 9060, 9061, 9430, 9443, 139, 50000, 50005, 3300 | Used for SAP and Maximo Interfaces. |
443, 8080, 8005, 7000, 7001, 7777, 7555,1099, 8040, 8101, 9001, 44444, 5432, 443, 61616, 5013 | Used for APM Interfaces. |
Other Considerations
Here are other requirements and information about installing Atoms:
- Multiple runtime environments can be installed on the same operating system
- A reliable high speed internet connection is required
- Network connectivity must be enabled between the source and destination systems
- The Atom installation path cannot contain unicode characters
- Installation should be executed running the installer as an administrator
- Ensure the OS hosting the Atom and any attached storage devices have synchronized system clocks